Other Parts Discussed in Thread: TDC1000-Q1, PGA460-Q1, TDC1000
As seen in part number TDC1000-Q1 has feature of TIme of Flight and PGA450-Q1 has Fullly Integrated feature. What is the difference between Fully Integrated and Time of Flight?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As seen in part number TDC1000-Q1 has feature of TIme of Flight and PGA450-Q1 has Fullly Integrated feature. What is the difference between Fully Integrated and Time of Flight?
HI Nihar,
The "fully integrated" aspect of the PGA family refers to the integrated digital signal processing block of the PGA450-Q1, which performs the digital filtering and echo envelope generation from the raw ultrasonic signal. By generating the echo envelope, the device is then able to find the time-of-flight through threshold comparison, and report the time-of-flight value to the master controller.
Both the PGA and TDC devices include some amount of analog front end gain to normalize the ultrasonic echo; however, the TDC1000 is only able to generate zero-crossing based pulses using a subset of the threshold capabilities that the PGA450-Q1 is otherwise able to offer with greater flexibility and resolution. I recommend that you consider the latest ultrasonic sensing device, the PGA460-Q1, which offers superior performance, lower cost, and a smaller package compared to the older PGA450-Q1.