This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Flashing the FPGA with mmWave Studio 2.1 and Diamond Programmer 3.11.1.441.0

Part Number: DCA1000EVM


Hi all, I wanted to pass along some differences I observed between the DCA1000EVM User Guide and the latest versions of mmWave Studio and LATTICE Diamond Programmer. All of the below pertain to Section 9.2 in the User Guide.

  1. The FPGA firmware image is now located in a different folder than before: C:/TI/mmwave_studio_02_01_00_00/mmWaveStudio/PlatformBinaries/DCA1000FPGA (6c)
  2. The SPI flash device no longer has the prefix 'SPI-' (6d)

I believe thees are the only two. Minor overall, but figured I would share.

Bill