This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2080: Measurment time

Part Number: HDC2080

Hello,
what is the complete measurment time in case a change in the humidity? Do we have any app notes?

Regards, Holger

  • Dear Holger - 

    The conversion (or measurement) time per sample depends on the bits of resolution the device has been set for. For example, 14 bit conversion time for temp + humidity would be typically taking 610uSec + 660uSec for ~1270uSec, 11 bit would be total ~750uSec and and 9 bit total time would be around 500uSec.

    Here you can see where I stepped a chamber in 2.5%RH increments over time (units are seconds) and the HDC2080 performed well, responding to the chamber step changes quickly. 

        

  • Hello Josh,
    is there no settle time for the polyimide? What is the settle time from 0%RH to 100%RH or from 20%RH to 80%RH?

    Regards, Holger

  • Holger - 

    Typical response time for the range is at 8 seconds in the datasheet - normally we wait at least about 10-20 minutes for chamber to settle.