This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Does lab0010-gesture-recog-swipe demo support 1~3m range?

Genius 13655 points
Part Number: IWR1443


Hello Champs,

The lab0010-gesture-recog-swipe demo is configured to detect gestures within 0.35m of the IWR1443boost EVM. Can the demo support 1~3m range? If not, do we have other demo can support this range?

Thanks.
Rgds
Shine
  • Former Member
    0 Former Member

    Hello,

    We do not have a gesture recognition demo that is setup to support 1-3m range. The user will need to recollect data and train for the longer range use case.

    Amanda