Other Parts Discussed in Thread: FDC1004
Dear Sir/Madam,
How many custom sensor can I connected to FdC1004evm?
There is only 2 shield connection, that means I can only connect to two copper sensor? Because the one copper sensor had to connect to CLN1 and SHLD1, and another had to be connected to CLN2 and SHLD2?
Do I need to break off section 3 in order for me to connect the sensors?
Best Regards,
QiuPing Wang