This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Cannot connect to IWR6843AOPEVM

Part Number: IWR6843AOPEVM

Hi,

I am setting up a new IWR6843AOPEVM board with demo firmware. Now I could successfully flash in the AoP_Demo bin file from IWR64xx folder in SDK 3.2, but when trying to connect the device from mmWave Demo Visualizer, it always stuck at the step showing below. I have double check the SOP switches with all OFF ( which should mean function mode I assume ). And I have tried to connect it in Windows 10 and MacOS but neither of them works.

Is there any other things I need to concern?