This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MMWCAS-DSP-EVM: VPS set max frame size failed.

Part Number: MMWCAS-DSP-EVM

Tool/software: TI C/C++ Compiler

Hi Team,

     I am using the cascading radar evm. I set the radar width to be 512, radar height to be 64 and transferFmtPkt0 to be 6 (CP_ADC). Then I got the following errors:

captdrv/src/vpsdrv_captureCore.c @ Line 643:

Core control: Set Max Frame Size failed!!

Assertion @ Line: 384 in captureLink_drv.c: status == FVID2_SOK : failed !!!

Can I know what is the reason of this issue?

Thanks,

Frank