I have a machine and I want to keep the Z head a fixed distance above the material as I move the Z head in the XY plane without touching the surface.
I've successfully done this using a LDC1000 and a coil for metal objects eg if I move the head up then the LDC1000 gives me a reliable reading difference so I am able to maintain a position of say 1mm above the surface at all times even if the surface is curved or bowed. In this case, I wrapped a coil and the inductor coil was the sensor.
I want to do the same thing but make it work for both metallic and non-metallic objects so look to the FDC2214EVM.
However, I am a bit confused how to make this work. The idea I understand is there are two pins that form two plates eg a ground plate and a sensor plate. On the EVM, the sensor plate is a copper pad on the PCB bu the ground is disconnected? Why is the ground disconnected eg where is the second plate?
For my application, can I use any metal object as the sensor eg can I use a metal cone or rod does it have to be a flat plate?
Do I just leave the ground disconnected or should I connect it to the machine body? The machine body is all metal and the surface I'm trying to detect sits inside the machine. If the object is conductive, do I need to insulate the object from the machine body otherwise wouldn't it just be grounded to the rest of the machine and undetectable?
Thank you for any suggestions.