Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843AOP
Hi,
I wander if there is any chance I can use IWR6843AOP+MMWAVEICBOOST+DCA1000 to capture real-time data?
I use mmWave Studio. If I use the ContStream tap, the 6843AOP only transmit single frequency continuous signal but not chip signal. And ContStream always cause DCA1000 DDR and FPGA full problem.
I also tried set the Number of Frames to 0 in SensorConfig Tab. This can make platform run continuously, but it only send out the data to PC when the data file reaches 1GB.
I wonder if there is any way I can use to capture real-time data from the sensor while the platform transmit chirp signal.
Best,
Fangzheng