This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM75A: I2C Communication failed after few hour

Part Number: LM75A

Dear supporting team,

I've problem with LM75A which i2c communication failed after few hours, I work with linux OS environment and coding C to read i2c bus and calculate temperature value using LM75. Main board is a custom board using SAM9 with Linux OS, using it's i2c bus connected to LM75.

There is 10K resistor on both lines, and after just hard reset, i2c bus starts working again and linux OS soft reset has no change in i2c stuck state. I also change Lm75A chips several times and after that i change my base board but there is no changes in our state, i2c reading stops working after 2 or 3 hours. Temperature read 1 time per second.

BR, 

Masood,