This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200: TDC7200 when to do the calibration

Part Number: TDC7200


when does the TDC7200  perform the calibration to create the data for registers CALIBRATION1 and CALIBRTION2?

Is it automatically performed before every new measurement after setting up the START_MEAS to be 1 in the Config1 ?

thanks

Zhang