Other Parts Discussed in Thread: IWR1642
I recently watched the youtube marketing video for the 6843AOP webinar where it was claimed that people detection can occur at a maximum of 12m or 15m depending on whether MIMO or TX Beam steering is used.
My question is what is the minimum distance at which an adult can be unambiguosly detected by the AOP device at bore sight. What height should the AOP device be positioned to achieve this. Assuming it is NOT over head (i.e ceiling ) mounted.