This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: Object data over can

Part Number: AWR1443BOOST
Other Parts Discussed in Thread: AWR1642, AWR1443, MMWAVE-SDK

Hi,

I want to send data related to detected object over can port. I referred tirex where demo for object data over can has been given for AWR1642 ES2.0. But I have AWR1443 ES3.0. So what procedure do I need to follow in order to make this demo working for AWR1443 ES3.0?

Regards,

Rajeshwari

  • Rajeshwari,

    The Object data over CAN on AWR1642 uses the CANFD interface for CAN communication. This application cannot be used on the AWR1443.

    The AWR1443 does not have the CANFD interface. It only has a CAN interface. You will need to re-write the application using the CAN driver as reference from the MMWAVE-SDK.

    BR,

    Raghu