This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: Problems using zone occupancy 14xx

Part Number: AWR1443BOOST
Other Parts Discussed in Thread: IWR1443BOOST, , UNIFLASH, AWR1443, IWR1443

Hi,

I've already use the 1243/1443-EVM PROC010 REV A with the binary fournished by you (mmwave_industrial_toolbox_3_6_1). This means that I know how to program the board by using the jumper on SOP2 (after a successful upload I unplug the jumper. Everything worked find, suddenly the board stop working so I bought 2 boards:

- IWR1443BOOST REV B

- AWR1443BOOST REV B

I tried to use the same binary, but I wasn't able to program the boards. So I update all the software Uniflash and I use the mmwave_industrial_toolbox_4_0_1. Nevertheless, I wans't able to upload the binary. I always get:

[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Initialization complete.
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Flashing process starting...
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Connecting to COM Port COM26...
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Reset connection to device
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Set break signal
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Connection to COM port succeeded. Flashing can proceed.
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Reading device version info...
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: ** 2 files specified for flashing.
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Checking file C:/ti/mmwave_industrial_toolbox_4_0_1/labs/area_scanner/14xx_zone_occ/prebuilt_binaries/xwr12xx_xwr14xx_radarss.bin for correct header for AWR1443.
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Header of C:/ti/mmwave_industrial_toolbox_4_0_1/labs/area_scanner/14xx_zone_occ/prebuilt_binaries/xwr12xx_xwr14xx_radarss.bin file indicates it is not a valid file to flash to AWR1443: 0xb55a03d1L
[5/11/2019 15:22:43] [ERROR] Cortex_R4_0: !!! Aborting flashing of specified files!!!
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Disconnecting from device on COM port COM26...
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
[5/11/2019 15:22:43] [INFO] Cortex_R4_0: Instance deinitialized!
I checked the port COM UART, the jumper and I power it with 5v 5A.
I thank you for all your help.
Best regards,
Jorge TAPIA.