This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: MMWAVEICBOOST

Part Number: IWR6843ISK
Other Parts Discussed in Thread: MMWAVEICBOOST

I am working with IWR6843ISK connected to MMWAVEICBOOST

Is there a liberay or an example code for raspberry pi4 to detect, if a person is 2m or 4 m in front of the sensor? Best will be, if this works with python.