Hi,
We are trying to build the image from the mmWave Studio.
Compiling Vision SDK 3.7 using tda2xx_cascade_linux_radar and RADAR_STUDIO=yes is successful but when trying to connect to it from mmWave Stdio using the Cascade_Configuration_MIMO.lua script fails.
We were able to use a precompiled SD card image with mmWave Studio using the same script but would like to have the flexibility to compile and modify it - which currently does not work.
Note that in the communication it appears that when the SD card communicates with mmWave Studio it reports VISION_SDK_03_07_01_00. It appears the latest version available on your website is Vision SDK 3.07.00.00 from June 2019.
How can we build the Vision SDK so it would work with mmWave Studio?
If a new Vision SDK is required, where can we download it?
Many thanks,
Rani