This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: IWR1443 Self Start Working (standalone) - Re:IWR1642 Self Start Working (standalone)

Part Number: IWR1443


Dir Ti;

I'm now working with IWR1443BOOST under sdk210 environment.

I have questions regarding the standalone operation.

Along with the guidance on this form, I replaced cli.c with the one which includes commands and ifdef  statements.

The compile was successful but the code doesn't work well. The condition is following....

- When sensor starts, command port outputs;

Debug: Init Calibration Status = 0x11e

Error -1

- Next, Sensor stops and again sensor starts;

Error -1

Exeption: ../sensor_mgmt.c line 467

By tracing source code, the problem seems to be a mismatching in memcmp() in line 460 of sensor_mgmt.c

Please show how to fix this problem.

Thanks in advance,

Kaneko

  • Former Member
    0 Former Member

    Hello,

    Can you provide some more details:

    1 Using the example cli.c provided in the thread are you able to compile for stand alone mode? Or have you just seen the issue with your custom cli.c file? .

    2. Have you checked that the config file you are trying to hard code works when you load it through the CFG port?

    3. Can you post your modified cli.c file to check for errors?

    Amanda

  • Dear Amanda-san;

    Thank you for your support.

    What I did so far is as following;

    (1) and (2)

    - The compilation of the original mmw_demo application was OK under CCS 910 environment. And the operation of this module with 'mmwDemo visualizer' is also OK.

    - I designed 'fluid level sensor '-like application by VB (because the 'mmw_high_accu_14xx' module compiled under sdk210 seems not to be correctly connected with fluid level sensor web application.)

      The compiled mmw_demo module works OK with 'fluid level sensor '-like application (data port) and terminal software (Tera term) (user UART).

    - Next, I replaced the orignal cli.c with sland-alone cli.c (command set is replaced to the one extracted  by 'mmwDemo visualizer'). Compilation was successfully ended.

    - I ran this stand-alone module and then connects VB application and Tera term to the module. The module seems not to operate. 

      I issued sensorStop and sensorStart commands. Then the module outputs "Error -1   (CR/LF) Exeption: ../sensor_mgmt.c line 467"

    - I removed sensorStart command from sland-alone cli.c and mannualy start the module. Then the module outputs "Debug: Init Calibration Status = 0x11e (CR/LF) Error -1"

    In both case the root cause seems to be a mismatching in memcmp() in line 460 of sensor_mgmt.c as I confirmed it by varying return codes in suspicious positions of the program.

    (3)

    I attached 'sland-alone cli.c' ( no changes essentially).

    I have related questions.

    As If-clause of 'sensor_mgmt.c' seems to be detecting mismatch or change of openCfg after Mmw=open() is called for the first time, in this case (in stand-alone application,

    config is set only once) this part of checking seems not to be necessary. Is it correct?

    Is this issue particular to sdk210?  As the original 'sland-alone cli.c' is dedicated to sdk120. 

    Thanks,

    Kaneko.

    **

    /*
     *   @file  cli.c
     *
     *   @brief
     *      CLI Utility implementation
     *
     *  \par
     *  NOTE:
     *      (C) Copyright 2016 Texas Instruments, Inc.
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /**************************************************************************
     *************************** Include Files ********************************
     **************************************************************************/
    
    /* Standard Include Files. */
    #include <stdint.h>
    #include <stdlib.h>
    #include <stddef.h>
    #include <string.h>
    #include <stdio.h>
    
    /* BIOS/XDC Include Files. */
    #include <xdc/std.h>
    #include <ti/sysbios/knl/Task.h>
    
    /* mmWave SDK Include Files: */
    #include <ti/common/sys_common.h>
    #include <ti/drivers/uart/UART.h>
    #include <ti/utils/cli/cli.h>
    #include <ti/utils/cli/include/cli_internal.h>
    
    /**************************************************************************
     *************************** Hard-coded Configuation **********************
     **************************************************************************/
    #define USE_HARD_CODED_CONFIG
    
    #ifdef USE_HARD_CODED_CONFIG
    
    int32_t hardCodedConfigIndex;
    
    char * hardCodedConfigCommands[] =
    {
     "% ***************************************************************",
     "% Created for SDK ver:01.02",
     "% Created using Visualizer ver:2.0.0.2",
     "% Frequency:77",
     "% Platform:xWR14xx",
     "% Scene Classifier:best_range_res",
     "% Azimuth Resolution(deg):15",
     "% Range Resolution(m):0.044",
     "% Maximum unambiguous Range(m):9.01",
     "% Maximum Radial Velocity(m/s):1",
     "% Radial velocity resolution(m/s):0.13",
     "% Frame Duration(msec):100",
     "% Range Detection Threshold (dB):15",
     "% Range Peak Grouping:enabled",
     "% Doppler Peak Grouping:enabled",
     "% Static clutter removal:disabled",
     "% ***************************************************************",
     "sensorStop",
     "flushCfg",
     "dfeDataOutputMode 1",
     "channelCfg 2 1 0",
     "adcCfg 2 1",
     "adcbufCfg 0 1 0 1",
     "profileCfg 0 77 916 7 57.14 0 0 70 1 240 4884 0 0 30",
     "chirpCfg 0 0 0 0 0 0 0 1",
     "chirpCfg 1 1 0 0 0 0 0 0",
     "frameCfg 0 0 16 0 100 1 0",
     "lowPower 0 1",
     "%guiMonitor 1 1 0 0 0 0",
     "cfarCfg 0 2 8 4 3 0 1280",
     "peakGrouping 1 1 1 1 229",
     "multiObjBeamForming 1 0.5",
     "clutterRemoval 0",
     "calibDcRangeSig 0 -5 8 256",
     "compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0",
     "measureRangeBiasAndRxChanPhase 0 1.5 0.2",
     "CQRxSatMonitor 0 3 5 123 0",
     "CQSigImgMonitor 0 119 4",
     "analogMonitor 1 1",
     "%sensorStart",
     "!!!END_OF_HARD_CODED_COMMANDS"
    };
    
    #endif
    
    /**************************************************************************
     *************************** Global Variables *****************************
     **************************************************************************/
    
    /**
     * @brief   Global variable which tracks the CLI MCB
     */
    CLI_MCB     gCLI;
    
    /**************************************************************************
     **************************** CLI Functions *******************************
     **************************************************************************/
    
    /**
     *  @b Description
     *  @n
     *      The function is the HELP generated by the CLI Module
     *
     *  \ingroup CLI_UTIL_INTERNAL_FUNCTION
     *
     *  @retval
     *      Not Applicable.
     */
    static int32_t CLI_help (int32_t argc, char* argv[])
    {
        uint32_t    index;
    
        /* Display the banner: */
        CLI_write ("Help: This will display the usage of the CLI commands\n");
        CLI_write ("Command: Help Description\n");
    
        /* Cycle through all the registered CLI commands: */
        for (index = 0; index < gCLI.numCLICommands; index++)
        {
            /* Display the help string*/
            CLI_write ("%s: %s\n",
                        gCLI.cfg.tableEntry[index].cmd,
                       (gCLI.cfg.tableEntry[index].helpString == NULL) ?
                        "No help available" :
                        gCLI.cfg.tableEntry[index].helpString);
        }
    
        /* Is the mmWave Extension enabled? */
        if (gCLI.cfg.enableMMWaveExtension == 1U)
        {
            /* YES: Pass the control to the extension help handler. */
            CLI_MMWaveExtensionHelp ();
        }
        return 0;
    }
    
    /**
     *  @b Description
     *  @n
     *      This is the CLI Execution Task
     *
     *  \ingroup CLI_UTIL_INTERNAL_FUNCTION
     *
     *  @retval
     *      Not Applicable.
     */
    static void CLI_task(UArg arg0, UArg arg1)
    {
        uint8_t                 cmdString[256];
        char*                   tokenizedArgs[CLI_MAX_ARGS];
        char*                   ptrCLICommand;
        char                    delimitter[] = " \r\n";
        uint32_t                argIndex;
        CLI_CmdTableEntry*      ptrCLICommandEntry;
        int32_t                 cliStatus;
        uint32_t                index;
    
        /* Do we have a banner to be displayed? */
        if (gCLI.cfg.cliBanner != NULL)
        {
            /* YES: Display the banner */
            CLI_write (gCLI.cfg.cliBanner);
        }
    
    #ifdef USE_HARD_CODED_CONFIG
        hardCodedConfigIndex = 0;
        CLI_write ("Wait some time for system to initialize...\n");
        Task_sleep(100);
        CLI_write ("Performing hard-coded config\n");
    #endif
    
        /* Loop around forever: */
        while (1)
        {
            /* Demo Prompt: */
            CLI_write (gCLI.cfg.cliPrompt);
    
            /* Reset the command string: */
            memset ((void *)&cmdString[0], 0, sizeof(cmdString));
    
    #ifdef USE_HARD_CODED_CONFIG
            /* Run hard-coded commands, one at a time until '!!!END_OF_HARD_CODED_COMMANDS' is reached: */
            if (hardCodedConfigCommands[hardCodedConfigIndex][0] != '!')
            {
                //CLI_write (hardCodedConfigCommands[hardCodedConfigIndex]);
                CLI_write ("Command\n");
                memcpy((void *)&cmdString[0], (void *)hardCodedConfigCommands[hardCodedConfigIndex], strlen(hardCodedConfigCommands[hardCodedConfigIndex]));
                hardCodedConfigIndex++;
            }
            /* Accept commands from UART after all hard-coded commands done: */
            else
            {
                /* Read the command message from the UART: */
                UART_read (gCLI.cfg.cliUartHandle, &cmdString[0], (sizeof(cmdString) - 1));
            }
    
    #else
            /* Read the command message from the UART: */
            UART_read (gCLI.cfg.cliUartHandle, &cmdString[0], (sizeof(cmdString) - 1));
    #endif
    
            /* Reset all the tokenized arguments: */
            memset ((void *)&tokenizedArgs, 0, sizeof(tokenizedArgs));
            argIndex      = 0;
            ptrCLICommand = (char*)&cmdString[0];
    
            /* comment lines found - ignore the whole line*/
            if (cmdString[0]=='%') {
                CLI_write ("Skipped\n");
                continue;
            }
    
            /* Set the CLI status: */
            cliStatus = -1;
    
            /* The command has been entered we now tokenize the command message */
            while (1)
            {
                /* Tokenize the arguments: */
                tokenizedArgs[argIndex] = strtok(ptrCLICommand, delimitter);
                if (tokenizedArgs[argIndex] == NULL)
                    break;
    
                /* Increment the argument index: */
                argIndex++;
                if (argIndex >= CLI_MAX_ARGS)
                    break;
    
                /* Reset the command string */
                ptrCLICommand = NULL;
            }
    
            /* Were we able to tokenize the CLI command? */
            if (argIndex == 0)
                continue;
    
            /* Cycle through all the registered CLI commands: */
            for (index = 0; index < gCLI.numCLICommands; index++)
            {
                ptrCLICommandEntry = &gCLI.cfg.tableEntry[index];
    
                /* Do we have a match? */
                if (strcmp(ptrCLICommandEntry->cmd, tokenizedArgs[0]) == 0)
                {
                    /* YES: Pass this to the CLI registered function */
                    cliStatus = ptrCLICommandEntry->cmdHandlerFxn (argIndex, tokenizedArgs);
                    if (cliStatus == 0)
                    {
                        CLI_write ("Done\n");
                    }
                    else
                    {
                        CLI_write ("Error %d\n", cliStatus);
                    }
                    break;
                }
            }
    
            /* Did we get a matching CLI command? */
            if (index == gCLI.numCLICommands)
            {
                /* NO matching command found. Is the mmWave extension enabled? */
                if (gCLI.cfg.enableMMWaveExtension == 1U)
                {
                    /* Yes: Pass this to the mmWave extension handler */
                    cliStatus = CLI_MMWaveExtensionHandler (argIndex, tokenizedArgs);
                }
    
                /* Was the CLI command found? */
                if (cliStatus == -1)
                {
                    /* No: The command was still not found */
                    CLI_write ("'%s' is not recognized as a CLI command\n", tokenizedArgs[0]);
                }
            }
        }
    }
    
    /**
     *  @b Description
     *  @n
     *      Logging function which can log the messages to the CLI console
     *
     *  @param[in]  format
     *      Format string
     *
     *  \ingroup CLI_UTIL_EXTERNAL_FUNCTION
     *
     *  @retval
     *      Not Applicable.
     */
    void CLI_write (const char* format, ...)
    {
        va_list     arg;
        char        logMessage[256];
        int32_t     sizeMessage;
    
        /* Format the message: */
        va_start (arg, format);
        sizeMessage = vsnprintf (&logMessage[0], sizeof(logMessage), format, arg);
        va_end (arg);
    
        /* Log the message on the UART CLI console: */
        if (gCLI.cfg.usePolledMode == true)
        {
            /* Polled mode: */
            UART_writePolling (gCLI.cfg.cliUartHandle, (uint8_t*)&logMessage[0], sizeMessage);
        }
        else
        {
            /* Blocking Mode: */
            UART_write (gCLI.cfg.cliUartHandle, (uint8_t*)&logMessage[0], sizeMessage);
        }
    }
    
    /**
     *  @b Description
     *  @n
     *      This is the function which is used to initialize and setup the CLI
     *
     *  @param[in]  ptrCLICfg
     *      Pointer to the CLI configuration
     *
     *  \ingroup CLI_UTIL_EXTERNAL_FUNCTION
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   <0
     */
    int32_t CLI_open (CLI_Cfg* ptrCLICfg)
    {
        Task_Params     taskParams;
        uint32_t        index;
    
        /* Sanity Check: Validate the arguments */
        if (ptrCLICfg == NULL)
            return -1;
    
        /* Initialize the CLI MCB: */
        memset ((void*)&gCLI, 0, sizeof(CLI_MCB));
    
        /* Copy over the configuration: */
        memcpy ((void *)&gCLI.cfg, (void *)ptrCLICfg, sizeof(CLI_Cfg));
    
        /* Cycle through and determine the number of supported CLI commands: */
        for (index = 0; index < CLI_MAX_CMD; index++)
        {
            /* Do we have a valid entry? */
            if (gCLI.cfg.tableEntry[index].cmd == NULL)
            {
                /* NO: This is the last entry */
                break;
            }
            else
            {
                /* YES: Increment the number of CLI commands */
                gCLI.numCLICommands = gCLI.numCLICommands + 1;
            }
        }
    
        /* Is the mmWave Extension enabled? */
        if (gCLI.cfg.enableMMWaveExtension == 1U)
        {
            /* YES: Initialize the CLI Extension: */
            if (CLI_MMWaveExtensionInit (ptrCLICfg) < 0)
                return -1;
        }
    
        /* Do we have a CLI Prompt specified?  */
        if (gCLI.cfg.cliPrompt == NULL)
            gCLI.cfg.cliPrompt = "CLI:/>";
    
        /* The CLI provides a help command by default:
         * - Since we are adding this at the end of the table; a user of this module can also
         *   override this to provide its own implementation. */
        gCLI.cfg.tableEntry[gCLI.numCLICommands].cmd           = "help";
        gCLI.cfg.tableEntry[gCLI.numCLICommands].helpString    = NULL;
        gCLI.cfg.tableEntry[gCLI.numCLICommands].cmdHandlerFxn = CLI_help;
    
        /* Increment the number of CLI commands: */
        gCLI.numCLICommands++;
    
        /* Initialize the task parameters and launch the CLI Task: */
        Task_Params_init(&taskParams);
        taskParams.priority  = gCLI.cfg.taskPriority;
        taskParams.stackSize = 4*1024;
        gCLI.cliTaskHandle = Task_create(CLI_task, &taskParams, NULL);
        return 0;
    }
    
    /**
     *  @b Description
     *  @n
     *      This is the function which is used to close the CLI module
     *
     *  \ingroup CLI_UTIL_EXTERNAL_FUNCTION
     *
     *  @retval
     *      Success -   0
     *  @retval
     *      Error   -   <0
     */
    int32_t CLI_close (void)
    {
        /* Shutdown the CLI Task */
        Task_delete(&gCLI.cliTaskHandle);
    
        /* Cleanup the memory */
        memset ((void*)&gCLI, 0, sizeof(CLI_MCB));
        return 0;
    }
    
    

  • Dear Amanda-san;

    I have to apologize you.

    The situation is that I thought the modified cli.c had been compiled when I rebuilt the project under ccs, but I found after some experiment that cli.c was out of rebuilt range.

    After I compiled cli.c locally, I could successfully built the stand-alone demo application and confirmed correct operation.

    Anyway, thank you very much for your support.

    -Kaneko.