Other Parts Discussed in Thread: MMWAVE-DFP
Hi,
My customer would like to use AWR1243P to enable cascade feature on their custom board and I got some questions from them:
1) AWR1243P is performance variant of AWR1243 and the main differences of the features between AWR1243P and AWR1243 are, for example, the number of simultaneous Tx channel and cascading option. My understanding is that the chip itself is exactly same between them and TI additionally tests and characterizes AWR1243P to support these features for the performance. Correct, right ?
2) In case of AWR1243, we need a firmware from the MMWAVE-DFP package. How about the case of AWR1243P cascading ? Can we suppose to use the same firmware ( MMWAVE-DFP package for AWR1243) on AWR1243P and that is still needed to deploy on the external QSPI Flash ? Or, do you have a specific firmware for AWR1243P ?
Best Regards,
NK