Hello,
query 1 : Please verify the configuration for external triggering and corresponding software settings for IWR1443boost.
Software configuration: Setting as external trigger in configuration file.
Hard ware configuration : By Applying 100ns pulse of 3.3v at pin 16 of J1 (60 pin connector) . (Example, Can we apply pulse of Arduino )
query 2 : IN the link https://e2e.ti.com/support/sensors/f/1023/t/734332?IWR1443BOOST-How-do-you-connect-external-hardward-trigger-
it is mentioned that "sheet 3 - goes to U2 ball N10 IWR1443 Mmwave sensor (you need to use R62 or R165 for monitoring, there are no other components"
can you please elaborate it .
what is ment by you need to use R62 or R165 for monitoring. and goes to U2 ball N10, such info not included in IWR1443BOOST_RevA_schematics and what is monitoring ?
query 3 : How to know absence of R165 in our board.
query 5: what is input impedance of the pin 16 of J1 connector and current specification for the pulse. ( any previous buffer circuit needed ? )
query 6: we have dca1000 , we need one more samtech cable for QSH-030-01-L-D-A , can you please share the details of the cable send along with the DCA1000 and where can we buy it ?
thanks and regards
Siddesh.B.M