This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Device capability questions.

Part Number: AWR1642

Hi team,

I am working with a customer on this device, and have some questions on the capability of this device (open to suggestions on a different device as well if its better suited):

1. Does the chip-set have provision for both up-and down-chirps?  If so, is the time lag between conclusion of up-chirp and commencement of down-chirp programmable?

2. Can baseband processing be adapted to handle direct and inverted downconversion spectra?

3. Recognizing that automotive applications have update times in the order of 40 to 60 ms, can the processor (for up to 6 point scatterers) handle update times that are shorter by 8X? 16X? 24X?