This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200: CSB of TDC7200

Part Number: TDC7200

Hi:

   If  only one TDC7200 is used for the product, can we just connect the CSB pin to the circuit GND all the time?

thanks

Zhang

  • Zhang,

    Yes, if using only one TDC7200 you can assert the CSB pin to GND all the time.

    However CSB is an active-low signal and needs to be low throughout a transaction.De-asserting CSB always terminates an ongoing transaction, even if it is not yet complete. Re-asserting CSB will always bring the device into a state ready for the next transaction, regardless of the termination status of a previous transaction.