Hi,
I am trying to check if CAN port on my board is working or not. For that I got suggestion to use 'Unit Test code for CAN' under mmWave SDK.
I am flashing xwr14xx_can_mss.xer4f from C:\ti\mmwave_sdk_02_01_00_04\packages\ti\drivers\can\test\xwr14xx path in debug mode in CCS. But test is getting stuck, it's not even failing.
What can be the issue? Am I doing it in right way?
I am also confused about baud rate that is being used for test? I mean to say what baud rate do I need to set on receiving side? Is it 1Mbps?
As I am confused about baud rate I was just checking for loopback tests, but test is getting stuck just after showing different choices.
Regards,
Rajeshwari