Other Parts Discussed in Thread: AWR1642, AWR1642BOOST, AWR1243, , MMWCAS-DSP-EVM, MMWCAS-RF-EVM
Respected ,
After studying,working on AWR1243 boost and AWR1642 boost IQ signal processing i came to know that after considering all parameter of the EVM and signal processing advantage , disadvantages with single chips (AWR1243 boost , AWR1642boost ) is possible to detect low RCS target ( 0.5 m sq- 1m sq) up to 40m -50 m and not more than that , even we are able configure the device for long distance the gain of antennas will not supports to detect low RCS target at long ranges.
This is verified with many experiments and decided to purchase TIDEP-01012 ( MMWAVCAS-DSP-EVM and MMWAV-RF-EVM ) where it is able to detection Low RCS targets at 120 m ( My interest of work) with Tx beamforming method .
Please advice what best suit for my interest of work.
The implementation is advance and cost as well .
So i want to make sure all my doubts are clear before buying this particular EVM (TIDEP-01012) .
As mentioned in below document .
http://www.ti.com/lit/ug/tiduen5/tiduen5.pdf
Section 4.2.2.2,4.2.2.3,4.2.2.4,4.2.2.5 and 4.2.3.2.
Is there any tool box or application or matlab code are available to get similar kind of results/ plots which are shown in above link . Or we need to develop our own post processing code for this kind of results?
If we need to develop our own post processing algo what kind of materials that TI will provide ?
after installing mmwave_studio_02_01_00_00 version I have seen matlab codes related to 4 chip cascade version but don't know how to use ....So is there any tutorials regarding using ( for beginners)?
Using (TIDEP-01012) + mmwave_studio_02_01_00_00 related (starting) help ?
Live streaming of IQ data from sensor is possible ?
Please provide the answers to my doubts and help me
Thanks in advance !