Other Parts Discussed in Thread: UNIFLASH,
Hi,
I recently installed Uniflash 5.2 on my Mac computer running OSX (10.14.5 Mojave). I use Uniflash to load firmware to a custom board with an IWR6843 chip via serial connection. Everything works fine if I use Uniflash from Windows but from OSX I am unable to load the binary image. From what I see it looks to me the application is unable to connect to the device even if I specify the correct serial device (/dev/cu.usbserial-FTL6FQ3O in my case)
This is the Uniflash log:
15:47:52:016 debug - Target Configuration. Device: iwr6843, Connection: Serial_Connection, LP: true
15:47:53:838 debug - ufDS, session.configured, partnum of current session = iwr6843
15:47:53:873 debug - addTargetStateListener on Cortex_R4_0
15:47:53:939 error - {}
15:49:07:341 error - {}
15:49:23:045 debug - returning new configure
15:49:23:381 debug - configured
15:49:23:418 debug - connect to core Cortex_R4_0
15:49:43:328 error - {}
I have the same error even if I run Uniflash as root.
Any idea?
Thanks,
Marco