Part Number: FDC2112
Hello
We are using the FDC2112 in a liquid level application. We are using a differential measurement, 2 plates inside a vessel and they have direct contact with the liquid, and the device and application is working.
However, we are having problem when trying to pass CE EMI certification since we get radiated emissions above the allowed level. Our investigations show the noise is coming from the sensor plates attached to FDC2112 and the noise disappears when FDC2112 stops it's measurements.
In addition, the harmonics are 16.8MHz multiples, roughly double the resonance frequency. Interestingly, the radiation is large when the sensor is dry. When we wet the sensor (ie, place liquid into the vessel), the noise reduces significantly , under the limit (and hence we can pass in that state).
I see in another forum post (Chris Oberhauser66 e2e.ti.com/.../2432400 there are 2 suggestions:
- ferrite beads in series between the FDC2112+LC tank, and the sensor
- And caps to ground from IN0x pins.
Our design aim was to reduce any parasitic capacitance or inductance attached to the circuit, but here I see additional inductance and capacitance being added.
Our circuit is as below :
We use the internal oscillator, but calibrate our measurement including the internal oscillator frequency on the production line.
1a/ Can you explain what purpose the ferrite beads perform?
1b/ Can you explain what purpose the cap to ground perform?
1c/ How should we chose the ferrite beads.
2/ Presumably our ESD clamp diodes will be functioning similar to the caps to ground? Although these components have around Cjunction = 0.5pF , so not 1/2 the nominal sensor capacitance (as mentioned in that post).
Our measurement range is typically 2-25pF sensor capacitance after calibration (including offset) . However, the offset capacitance is around 30pF.
2b/ Do I understand it correctly then that our nominal sensor capacitance is 30 + ((25-2)/2) = 41pF?
3/ Do you have any suggestions on how to reduce the radiated noise (in particular in our dry sensor case)?
4/ Can we adjust any registers to reduce the noise? I'm wondering if slowing down the sampling will reduce the average power output and therefore reduce the spikes? I guess I should also recheck the Vpk amplitude.
5/ Regarding the drive strength and oscillation amplitude, is it possible to increase the drive strength from small to large via SW, and monitor the Amplitude High and Low Warnings, and then select a mid-point drive strength between those? Algorithmically by SW that is possible, but in practice will that give a correct /sufficient drive strength?
Many thanks,
Hadyn van der Berg