This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Pin characteristics for NRESET(ball#R3)

Part Number: IWR6843
Other Parts Discussed in Thread: MMWAVEICBOOST

I am looking for information about the NRESET (ball#R3) input pin characteristics such as input current and presence of an internal pull-up or pull-down resistor.

I am referencing IWR6843 datasheet (SWRS219B, Sept 2019 revision) and I can't find this information. I don't see a spec for input current on any digital I/Os including NRESET. Also, the Reset pin (NRESET) is not included in Table 4-1.

From empirical measurements we believe the NRESET input may have a 30K ohm pull-down resistance to ground as we are measuring a 83uA current into the device when we pull the pin high. Is this expected?