This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Configure udp-packet size

Part Number: DCA1000EVM

Hi,

I have a related question on the "DCA1000EVM: Expected packet loss rate?" post.

I want to change the udp-package size by useing the udp command CONFIG_PACKET_DATA_CMD_CODE. In wireshark I can see my message beeing sent out to the DCA1000. I also get a response with no errors. But the package size is not changed. Is it possible to change the udp package size at all? 

The message in Wireshark looks like this: 5aa50b000600000000320200aaee

This is the response of the DCA1000: 5aa50b000000aaee

The red marked part is telling that everything should be allright. I also tried to change the message with its endianess, but nothing seems to change the package size.

Thanks for any help. 

Best regards,

Markus