Hi, I'm currently working on this project, which involves a measurement of sound signal using condenser microphone. Using the GUI provided with this sensor, I can maximize the sampling rate to be approximately 421kHz in the configuration setting, however, when I log the data in csv file, it can only log data up to 400 samples/sec (400Hz). Is there a way to maximize the data logging rate such that it can log as fast as 20kHz?
I will attach the user manual provided for this sensor below.
Thank you snou138a.pdf