Hello,
We're using the IWR1642BOOST to evaluate a long range tracking application. The SRR demo seems ideal, but I when I load the following cfg file into mmwave visualiser I get an invalid config. Do you have a working version that you can send me please?
We haven't changed the default .bin for the OOB demo, so it's using SDK v2.0. Also, I can't seem to set the range >50m inside the visualer, it would be interesting to see what exactly these settings are.
Regards,
Sanjeev.
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg 0 0 1 1
profileCfg 0 77 3 3 56 0 0 8 1 256 5000 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 64 0 100 1 0
lowPower 0 0
guiMonitor 1 1 1 0 0 1
cfarCfg 0 0 8 4 4 0 5000
cfarCfg 1 0 8 4 4 0 5000
peakGrouping 1 0 1 1 224
multiObjBeamForming 0 0.5
calibDcRangeSig 0 -5 8 256
sensorStart