I am doing a multi-mode radar and would like to use the Phase modulation capability of the device. Is this possible on the EVM and where do I find the instructions to do this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am doing a multi-mode radar and would like to use the Phase modulation capability of the device. Is this possible on the EVM and where do I find the instructions to do this?
Hi Cesar,
Thanks.
I am probably misunderstanding. I thought that, quite apart from the FMCW modulation, the TI devices support TDM and BPM- MIMO by the chirp pattern on the different TX antennae. Do we need for example a minimum of two radar devices ( e.g. AWR 1642) to do this or the chirp profile on each Tx antenna of a device is controllable?
Yes,
You are correct, TDM MIMO and BPM MIMO are supported. However the chirp is being transmitted using FMCW
Part of the chirp configuration the following can be configured (please check for example mmWave Studio Config GUI)
Thank you
Cesar
Thank you,
I will close this thread now.
If there are new questions please start a new thread
Cesar