Other Parts Discussed in Thread: IWR1443BOOST
Hi,
I'm trying to use DCA1000EVM with IWR1443BOOST on mmWave Studio 2.1.0.0. I have installed all the relevant software in mmWave Studio user guide, and DCA1000EVM user guide. My computer is connected to both of the devices, with static IP configured as given, and firewall disabled. I'm trying to use DataCaptureDemo_xWR.lua, as specified in the quick setup guide. When I run the lua script, everything seems to be working until start_command is sent. Then, I receive no of files captured is zero error. Here is the relevant part of logs:
[16:53:24] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[16:53:24] [RadarAPI]: Sending start_record command to DCA1000
[16:53:24] [RadarAPI]: Status: Passed
[16:53:25] [RadarAPI]: ar1.StartFrame()
[16:53:25] [RadarAPI]: Status: Passed
[16:53:25] Frame start async event received!
[16:53:25] [RadarAPI]: Frame Ended
[16:53:25] Frame End async event received!
[16:53:30] Please wait for a few seconds for matlab post processing .....!!!!
[16:53:30] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[16:53:30] [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8
[16:53:30] Error : The number of files captured is zero!
[16:53:40]
[16:53:40]
I've attached the rest of the logs as a separate file. This script automatically enables test source; by looking at some other threads on the forum, I've set disabled test source, and applied steps on SensorConfig page in the given order. I wait for a couple of seconds after clicking DCA1000ARM, and also tried adding RSTD.Sleep(2000) on Lua Shell after clicking DCA100ARM button, but it does not show up on the output log screen, and it does not seem to have any effect. Any help is appreciated.
GM: Constructor GM: Fri Nov 22 16:52:45 2019 RSTD.Transmit("/Settings") [16:52:45] [16:52:45] ### Running Startup script: "C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Scripts\Startup.lua" ### [16:52:45] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1") [16:52:45] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss") [16:52:45] Scripter ignored: Attempt to UnBuild() again or before Build. [16:52:45] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll") [16:52:45] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE") [16:52:45] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE") [16:52:45] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE") [16:52:45] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE") [16:52:45] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE") [16:52:45] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\RunTime\\SAL.dll") [16:52:45] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "") [16:52:45] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE") [16:52:45] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1") [16:52:45] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE") [16:52:45] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE") [16:52:45] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false") [16:52:45] RSTD.Transmit("/") [16:52:45] RSTD.SaveSettings(): Settings saved to "C:\Users\******\AppData\Roaming\RSTD\config.xml" [16:52:45] RSTD.Build() [16:52:45] RSTD.SaveSettings(): Settings saved to "C:\Users\*******\AppData\Roaming\RSTD\config.xml" [16:52:45] RSTD.Transmit("/") [16:52:45] RSTD.AL_Build() [16:52:45] RSTD.AL_LoadXml() [16:52:45] RSTD.Transmit("/") [16:52:45] RSTD.AL_Init() [16:52:45] RSTD.Clients_Build() [16:52:45] GM: Init [16:52:45] GM: Loaded 'C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Clients\\LabClient.dll' [16:52:45] GM: 1 Guest (s) init [16:52:45] GM: 1 Module(s) init [16:52:45] GM: 2 Tab (s) init [16:52:45] RSTD.Client_LoadXml() [16:52:45] [RadarAPI]: ar1.selectRadarMode(0) [16:52:45] [RadarAPI]: Status: Passed [16:52:45] Matlab Runtime Engine is installed [16:52:45] [RadarAPI]: Starting Matlab Engine.. [16:52:47] [RadarAPI]: Matlab Engine Started! [16:52:48] [RadarAPI]: ar1.selectCascadeMode(0) [16:52:48] [RadarAPI]: Status: Passed [16:52:48] [RadarAPI]: ar1.LoadSettings('C:\Users\*******\AppData\Roaming\RSTD\ar1gui.ini') [16:52:48] TESTING = false [16:52:48] RstdNet: Port 2777: Listening.. [16:52:48] [16:52:48] ***Script completed successfully.*** [16:52:57] [RadarAPI]: Opening Gpio Control Port() [16:52:57] [RadarAPI]: Status: Passed [16:52:57] [RadarAPI]: Opening Board Control Port() [16:52:57] [RadarAPI]: Status: Passed [16:52:58] [RadarAPI]: ar1.FullReset() [16:52:58] [RadarAPI]: Status: Passed [16:52:59] [RadarAPI]: Closing Board Control Port() [16:52:59] [RadarAPI]: Status: Passed [16:52:59] [RadarAPI]: Closing Gpio Control Port() [16:52:59] [RadarAPI]: Status: Passed [16:52:59] [RadarAPI]: ar1.SOPControl(2) [16:52:59] [RadarAPI]: Status: Passed [16:53:02] [RadarAPI]: ar1.Connect(3,921600,1000) [16:53:04] [RadarAPI]: Warning: Connected with baudrate 115200 [16:53:05] [RadarAPI]: Warning: Disconnected existing BaudRate [16:53:05] [RadarAPI]: Warning: Trying to connect with baudrate 921600 [16:53:07] [RadarAPI]: ar1.Calling_IsConnected() [16:53:08] [RadarAPI]: ar1.SelectChipVersion("AR1243") [16:53:08] [RadarAPI]: Status: Passed [16:53:08] [RadarAPI]: ar1.SelectChipVersion("AR1243") [16:53:08] [RadarAPI]: Status: Passed [16:53:08] [RadarAPI]: ar1.deviceVariantSelection("XWR1443") [16:53:08] [RadarAPI]: Status: Passed [16:53:08] [RadarAPI]: ar1.frequencyBandSelection("77G") [16:53:08] [RadarAPI]: ar1.SelectChipVersion("XWR1443") [16:53:08] [RadarAPI]: Status: Passed [16:53:08] Device Status : XWR1443/QM/SOP:2/ES:3 [16:53:08] [RadarAPI]: ar1.SaveSettings('C:\Users\*******\AppData\Roaming\RSTD\ar1gui.ini') [16:53:13] [RadarAPI]: ar1.ReadRegister(0xffffe214, 0, 31) [16:53:13] [RadarAPI]: ar1.ReadRegister(0xffffe210, 0, 31) [16:53:13] [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31) [16:53:13] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss.bin") [16:53:13] [RadarAPI]: Downloading BSS Patch RPRC Binary.. [16:53:15] [RadarAPI]: ar1.GetBSSFwVersion() [16:53:15] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17)) [16:53:16] [RadarAPI]: ar1.GetBSSPatchFwVersion() [16:53:16] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19)) [16:53:16] BSS FW Download Success [16:53:16] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss.bin") [16:53:16] [RadarAPI]: Downloading MSS RPRC Binary.. [16:53:19] [RadarAPI]: ar1.GetMSSFwVersion() [16:53:19] [RadarAPI]: MSSFwVersion:(01.02.05.01 (12/07/19)) [16:53:19] MSS FW Download Success [16:53:19] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0) [16:53:19] [RadarAPI]: Status: Passed [16:53:19] MSS power up done async event received! [16:53:19] Power On Success [16:53:20] [RadarAPI]: ar1.SelectChipVersion("AR1243") [16:53:20] [RadarAPI]: Status: Passed [16:53:20] [RadarAPI]: ar1.SelectChipVersion("XWR1443") [16:53:20] [RadarAPI]: Status: Passed [16:53:20] Device Status : XWR1443/QM/SOP:2/ES:3 [16:53:20] [RadarAPI]: ar1.RfEnable() [16:53:20] [RadarAPI]: Status: Passed [16:53:20] BSS power up done async event received! [16:53:21] [RadarAPI]: ar1.GetMSSFwVersion() [16:53:21] [RadarAPI]: MSSFwVersion:(01.02.05.01 (12/07/19)) [16:53:21] [RadarAPI]: ar1.GetBSSFwVersion() [16:53:21] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17)) [16:53:22] [RadarAPI]: ar1.GetBSSPatchFwVersion() [16:53:22] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19)) [16:53:22] RF Enable Success [16:53:22] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0) [16:53:22] [RadarAPI]: Status: Passed [16:53:22] ChanNAdcConfig Success [16:53:22] [RadarAPI]: ar1.LPModConfig(0, 0) [16:53:22] [RadarAPI]: Status: Passed [16:53:22] Regualar mode Cfg Success [16:53:22] [RadarAPI]: ar1.RfInit() [16:53:22] RF Init async event received! [16:53:22] [RadarAPI]: Time stamp, Temperture: 2050,36; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 0, 0; RxIQMM Status, Update: 1, 1; [16:53:22] [RadarAPI]: Status: Passed [16:53:22] RfInit Success [16:53:23] [RadarAPI]: ar1.DataPathConfig(1, 1, 0) [16:53:23] [RadarAPI]: Status: Passed [16:53:23] DataPathConfig Success [16:53:23] [RadarAPI]: ar1.LvdsClkConfig(1, 1) [16:53:23] [RadarAPI]: Status: Passed [16:53:23] LvdsClkConfig Success [16:53:23] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0) [16:53:23] [RadarAPI]: Status: Passed [16:53:23] LVDSLaneConfig Success [16:53:23] [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0) [16:53:23] [RadarAPI]: Status: Passed [16:53:23] Test Source Configuration Success [16:53:23] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30) [16:53:23] [RadarAPI]: Status: Passed [16:53:23] ProfileConfig Success [16:53:23] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0) [16:53:23] [RadarAPI]: Status: Passed [16:53:23] ChirpConfig Success [16:53:23] [RadarAPI]: ar1.EnableTestSource(1) [16:53:24] [RadarAPI]: Status: Passed [16:53:24] Enabling Test Source Success [16:53:24] Test Source Already Enabled...!!! [16:53:24] [RadarAPI]: ar1.EnableTestSource(1) [16:53:24] [RadarAPI]: Status: Passed [16:53:24] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1) [16:53:24] [RadarAPI]: Status: Passed [16:53:24] FrameConfig Success [16:53:24] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000") [16:53:24] [RadarAPI]: Status: Passed [16:53:24] SelectCaptureDevice Success [16:53:24] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098) [16:53:24] [RadarAPI]: Sending fpga command to DCA1000 [16:53:24] [RadarAPI]: [16:53:24] FPGA Configuration command : Success [16:53:24] [RadarAPI]: Sending fpga_version command to DCA1000 [16:53:24] [RadarAPI]: [16:53:24] [16:53:24] FPGA Version : 2.8 [Record] [16:53:24] [16:53:24] CaptureCardConfig_EthInit Success [16:53:24] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 1, 1, 2, 3, 0) [16:53:24] [RadarAPI]: Sending fpga command to DCA1000 [16:53:24] [RadarAPI]: [16:53:24] FPGA Configuration command : Success [16:53:24] CaptureCardConfig_Mode Success [16:53:24] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25) [16:53:24] [RadarAPI]: Sending fpga command to DCA1000 [16:53:24] [RadarAPI]: [16:53:24] FPGA Configuration command : Success [16:53:24] [RadarAPI]: Sending record command to DCA1000 [16:53:24] [RadarAPI]: [16:53:24] Configure Record command : Success [16:53:24] CaptureCardConfig_PacketDelay Success [16:53:24] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1) [16:53:24] [RadarAPI]: Sending start_record command to DCA1000 [16:53:24] [RadarAPI]: Status: Passed [16:53:25] [RadarAPI]: ar1.StartFrame() [16:53:25] [RadarAPI]: Status: Passed [16:53:25] Frame start async event received! [16:53:25] [RadarAPI]: Frame Ended [16:53:25] Frame End async event received! [16:53:30] Please wait for a few seconds for matlab post processing .....!!!! [16:53:30] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin") [16:53:30] [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8 [16:53:30] Error : The number of files captured is zero! [16:53:40] [16:53:40] ***Script completed successfully.*** [17:01:10] [RadarAPI]: ar1.DataPathConfig(1, 1, 0) [17:01:10] [RadarAPI]: Status: Passed [17:01:13] [RadarAPI]: ar1.LvdsClkConfig(1, 1) [17:01:13] [RadarAPI]: Status: Passed [17:01:13] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0) [17:01:13] [RadarAPI]: Status: Passed [17:01:16] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30) [17:01:16] [RadarAPI]: Status: Passed [17:01:19] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0) [17:01:19] [RadarAPI]: Status: Passed [17:01:20] [RadarAPI]: ar1.DisableTestSource(0) [17:01:20] [RadarAPI]: Status: Passed [17:01:20] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1) [17:01:20] [RadarAPI]: Status: Passed [17:01:23] [RadarAPI]: ar1.GetCaptureCardDllVersion() [17:01:23] [RadarAPI]: Sending dll_version command to DCA1000 [17:01:23] [RadarAPI]: [17:01:23] DLL Version : 1.0 [17:01:23] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000") [17:01:23] [RadarAPI]: Status: Passed [17:01:33] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1) [17:01:33] [RadarAPI]: Sending start_record command to DCA1000 [17:01:37] [RadarAPI]: ar1.StartFrame() [17:01:37] [RadarAPI]: Status: Passed [17:01:37] Frame start async event received! [17:01:37] [RadarAPI]: Frame Ended [17:01:43] [RadarAPI]: [17:01:43] Frame End async event received! [17:01:43] [RadarAPI]: [17:01:43] Start Record : [17:01:43] Timeout Error! System disconnected [17:01:45] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin") [17:01:45] [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8 [17:01:45] Error : The number of files captured is zero!