Hello Ti engineer
We are studying Azimuth MIMO and Elevation MIMO using MMWCAS-RF-EVM.
The virtual antenna of Azimuth MIMO is considered to be arranged as follows.
Is this recognition correct?
Also, when we check the Tx of MMWCAS-RF-EVM, we think that Elevation MIMO uses the following Tx(U1_4 Slave Tx1, U1_1 Master Tx3, Tx2, Tx1), RX ARRAY A.
When using these Tx and Rx, we think that the virtual antenna of Elevation MIMO is as follows.
Is this recognition correct?
In this case, we think that the antenna is not continuous in the elevation direction. Is this correct?
What should we do to complement between the antennas at this time?
Regards,
suzuki