This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200: TRIGG of TDC7200

Part Number: TDC7200

  Per the measurement sequence, after the start new measurement bit START_MEAS has been set in the CONFIG1 register, the TDC7200

generates a trigger signal on the TRIGG pin,  . Immediately after sending the trigger, the TDC7200 enables the START pin and waits to receive the START pulse edge.  . After receiving a START, the TDC resets the TRIGG pin

My question is: if no START signal arrive, the TRIGG pin will remain high all the time before interrupt occurs?

Thanks

Zhang