This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Programming / Initial Setup of new AWR1843BOOST based Development Board

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843

Hello,

We have created a custom development board based on the design files provided with the AWR1843BOOST Board, but with our own custom antenna design.

Since this board contains a TM4C1294NCPDTT3 MCU from TI, I assume needs to be flashed with specific firmware. Where can I find this firmware, and how is this typically loaded onto the MCU (programmer P/N)? Does the AWR1843 need to be flashed as well as part of initial board bring up?

From the schematics, the TM4C1294NCPDTT3  and the AWR1843 look to be on the same JTAG bus, which is connected to the large header. Does the programmer need to be wired to this connector to facilitate programming?

I have looked throughout the design resources, but I can not find any resources to help with this.

Thanks,

Andrew