This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1xxx Radar Interface Control Document

Hi Team,

The customer is experiencing below issue and needs your help.

MSGID corresponds to AWR_DEV_CONF_SET_MSG. But it should be corresponds to 0x1234 0x4321 and COMMAND type. The actual log information obtained is as follows:


[19:22:09:044]: Device [0] Host IRQ High

[19:22:09:045]: Device [0] [WR]0x5678 0x8765 0xFFFF 0xFFFF 0xFFFF 0xFFFF 0xFFFF 0xFFFF 

[19:22:09:047]: Device [0] Host IRQ Low
[19:22:09:048]: Device [0] [RD]0xDCBA 0xABCD
[19:22:09:048]: Device [0] [RD]0x8096[This does not correspond to the document, 0x202 MESGTYPE: 00 CMD instead of 01 RESPONSE] 0x000E 0x800C 0x0000 0x0000 0xFF4E
[19:22:09:048]: Device [0] [RD]0x2815

Is it a document error or a log error?

Thanks,

Annie