Hello, I am looking for guidance on programming very low data rates for the CAN-FD (MCAN) driver on AWR. In particular, 125kbps. Is this rate supported with the clock sources that are available on the device?
I found a generic timing calculator online, and it suggests it is possible to use a 40MHz input clock, but it doesn’t distinguish between the Prop_Seg and Phase_Seg_1 values I need to configure the driver.
http://www.bittiming.can-wiki.info/
Thanks
Bill