This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: AWR1642 Unable to boot

Part Number: AWR1642


Boot mode:101(SOP2~SOP0) AWR1642 Can be downloaded normally.

Boot mode:001(SOP2~SOP0) AWR1642 Unable to boot .

We have tested RESET and POWER rail to meet timing requirements.

SOP2~SOP0 Signal is ready when released RESET.

All supply voltages are normal

VOUT_14SYNTH output is 0V.

Is there any reason why AWR1642 cannot start normally?