Hi,
My application is to detect people within 50 m range with 40 degree or more azimuth angle. And I found this http://dev.ti.com/tirex/explore/node?node=AJymZUkImsF4knF6x3AKNg__VLyFKFf__LATEST by using IWR6843ISK. But I need to clarify the following things,
1) This lab ( http://dev.ti.com/tirex/explore/node?node=AJymZUkImsF4knF6x3AKNg__VLyFKFf__LATEST ) is designed for indoor conditions. But my requirement is for outdoors, is the same setup works fine for outdoors?
2) Is there any way to increase the range of detection to 70 meters?
3) If the system detected people then I need to blow an alarm, how can I do that? Is there any GPIO pins in the IWR6843ISK board to drive a relay for alarm?