Other Parts Discussed in Thread: AWR1843
Hey All,
So I'm working on a project to fuse a 140 FOV camera with the AWR1843. I have been using a tetrahedral corner detector as a target in order to relate both the sensors, but have faced a snag where I'm not able to generate points further than 2-3 meters from the radar without getting points from other objects.
I started looking onto active reflectors, and was wondering if you guys have any recommendation on buying an active reflector?
Also, can a signal generator, with a frequency range of 77 to 99 GHz, work as an Active reflector along with an antenna?
Regards.