Other Parts Discussed in Thread: IWR6843ISK, , MMWAVEICBOOST
Dear all,
I recently got IWR6843ISK + MMWAVEICBOOST + DCA1000EVM. The boards are powered from the MMWAVEICBOOST board (I use a lab power supply 5V, 5A).
I followed the "DCA1000EVM Quick Start Guide" and "DCA1000EVM Data Capture Card" user's guide but I have issue with the DCA1000EVM. I guess it is in controlling the Ethernet.
Those are the settings I'm using.
For MMWAVEICBOOST
For DCA1000EVM
Are those settings correct?
I have already programmed the FPGA SPI Flash using Lattice Diamond and DCA1000_FPGA_RECORD_V2.7_18JUN2018.bit
I got this issue when I try to click on "Connect, Reset and Configure":
Is it normal that the FPGA Version is 0.0.0.0? I programmed many times the FPGA SPI Flash but still the same issue.
I tried other configurations of the DCA1000EVM but the problem is still there. For example, I used HD_CONFIG (SW2.5), Loading the Ethernet configuration data from EEPROM (SW2.6 to USER_SW1), ...
This is when I try DataCaptureDemo_xWR:
If I click on (1) to (6), it seems working but still failing when I click "SetUP DCA1000".
Here are some screenshots of Wireshark:
Thanks a lot in advance.
Best Regards,
Marco