Hi
I want to read the raw ADC data while in continuous mode.
Is there any "Capture demo" for the IWR6843 somewhere I can use and modify as in the related post?
If so, where can i find it? I am a bit confused over the different names of all the different available pre-built software, OOB demos, Labs and Capture Demos, so please point me to a very specific place if there is any.
I am also working to get Mmwave Studio running on a Windows10 but are having issues with USB drivers (FTDI drivers, it seems this is a common problem looking here at the forum) so working in parallel on this way forward.
I have access to a boost board, and a DCA1000 and a antenna board of our own creation with the IWR6843 which can be connected to the DCA1000 board, and it works to stream raw data while in FMCW mode.
It is the last board I want to read raw adc data from while in CW mode.