Other Parts Discussed in Thread: AWR1642, IWR6843,
Starting with AWR1642, we changed the VitalSign on the algorithm side and was able to send the data output thru the UART to an external microcontroller succesfully. But we need to move to IWR6843ISK for regulatory compliance, so we started with the VitalSign codebase for IWR6843 that works well and copied the changes we did on the algorithm side, now the UART is throwing off (glitch) at random times and can't go more than 120s. On the prior AWR1642, we can run for 30min on this UART with no issue.
Note that I am using the mmwave SDK 3.1.1.2 and Industrial Toolbox 3.6.2 for IWR6843 ES1 chip. I am using the same SDK and Automotive Toolbox 2.5.0 for AWR1642 ES2 chip.
Here is the AWR1642 VitalSign profile we used (worked with no issue)
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 1 1 0
adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 77 7 6 57 0 0 70 1 100 2000 0 0 40
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 2 0 10 1 0
lowPower 0 1
guiMonitor 0 0 0 0 1
collectChirp 0
vitalSignsCfg 0.4 1.1 256 320 1 0.1 0.05 300000 300000
motionDetection 1 20 0.04 0
sensorStart
Now, for the new IWR6843 we are testing (worked but no more than 120s and it throws off UART at random times)
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 1 1 0
adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 60.25 7 6 57 0 0 65 1 100 2000 0 0 40
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 2 0 10 1 0
lowPower 0 1
guiMonitor 0 0 0 0 1
vitalSignsCfg 0.4 1.1 256 512 1 0.1 0.05 100000 300000
motionDetection 1 20 2.0 0
sensorStart
For reference, here are the TI provided profiles for AWR1642 and IWR6843 VitalSigns, respectively.
%TI AWR1642
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 2 0 50 1 0
lowPower 0 1
guiMonitor 0 0 0 0 1
calibDcRangeSig -1 0 0 0 0
vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000
motionDetection 1 20 2.0 0
sensorStart
%TI IWR6843
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 60.25 7 6 57 0 0 65 1 200 4000 0 0 40
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 2 0 50 1 0
lowPower 0 1
guiMonitor 0 0 0 0 1
calibDcRangeSig -1 0 0 0 0
vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000
motionDetection 1 20 2.0 0
sensorStart
Please critique our profiles for the before (AWR) and after (IWR) porting activity. Meanwhile, I will go debugging in the codebase if there is mistake made on porting activity.
Also, I saw the IWR6843 ES2 just came out, will this be more stable enough to solve this UART glitch issue?
Thanks so much guy for your work here.
Jonathan Ibera