I am using two tmp117 in my custom board design with one board A0 pin connected to the ground and other board A0 pin is pulled high. The board with the A0 pin connected to the ground works fine but when I try to address the other one with address 0x92, I am unable to read the chip ID. Is there an issue with my addressing or connection for the second tmp sensor?