This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP75: Translating binary to temperature

Part Number: TMP75


What equation is used to translate binary/hex readings to temperature readings?

 

  • /*
     *  ======== TMP75B_toIntCelsius ========
     *  Convert raw temperature register value to degrees Celsius rounded to the
     *  nearest integer
     */
    int32_t TMP75B_toIntCelsius(int32_t x)
    {
        /* Shift raw register value to form a proper Q4 value */
        x >>= 4;
    
        /* Optional: Add bias to round before the final truncation */
        x += (x >= 0) ? (1 << 3) : -(1 << 3);
    
        /* Convert Q4 value to whole number */
        x /= 1 << 4; /* use division so small negative values round to 0 */
    
        return x;
    }
    
    /*
     *  ======== TMP75B_toMilliCelsius ========
     *  Convert raw temperature register value to milli-degrees Celsius
     */
    int32_t TMP75B_toMilliCelsius(int32_t x)
    {
        /* Shift raw register value to form a proper Q4 value */
        x >>= 4;
    
        /* Scale to milli-degrees, convert Q4 value to a whole number */
        return ((1000 * x) >> 4);
    }
    
    /*
     *  ======== TMP75B_toFloatCelsius ========
     *  Convert raw temperature register value to degrees Celsius
     */
    float TMP75B_toFloatCelsius(int32_t x)
    {
        /* Shift raw register value to form a proper Q4 value */
        x >>= 4;
    
        /* Convert Q4 value to a float */
        return ((float)x * 0.0625f);
    }

    where input x is the two bytes read from I2C:

    x = (((int32_t)(int8_t)rxBuf[0]) << 8) | rxBuf[1];

    additionally, if only one byte is read, that byte is integer temperature in signed 8 bit format (signed char or similar.)