Hi Team
1. I would like to use a sensor for a mobile robot application where the obstacle tracking like glass and should be of minimum working range say like 20mm - 300mm distance. Would like to also know what is the minimum working range of this sensor, does the mmwave IWR6843 sensor have any blind spot region?. These info were not provided on the spec sheet.
2. Also there was a confusing thing that the angular area of coverage is 130deg and the resolution is 15deg, so do does this mean that we could get only 8 steps (130/15) of incremental angle data totally, ie; meaning it can only detect objects at 15deg, 30deg, 45deg, etc.. 130deg?
3. Also is there any limitation in packing the sensor on to the robot, say like should the entire board be exposed to the outer environment without covering it?
Please help me out with this query ASAP. Also we would like to have your suggestions on helping us out with any sensor with short working range which has a small blind spot and which can detect glass as well..
Thanks in advance!