This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004: Can FDC1004 used to sense solid particle level in plastic container?

Part Number: FDC1004
Other Parts Discussed in Thread: TIDA-00317, , TDC1000

Hi Team,

TIDA-00317 shows that FDC1004 can sense liquid level in the plastic container, now we have a similar application like this: the container is plastic, but the difference is that the things inside the container is unknown and may be liquid or solid particle such as seed or fruit(the diameter is within 10mm), so my questions are:

1. Can the solid particle level be sensed?

2. If the answer for item 1 is yes, how to calculate the level resolution?

Thanks and Best Regards!

Hao