This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: mmwave studio + DCA1000, timeout error

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843

Hi Expert,

I was trying to get raw data over LVDS through mmwave studio with IWR6843ISK module.

However, when I configured the module, I got the following error:

[15:33:11] [RadarAPI]: Opening Gpio Control Port()
[15:33:11] [RadarAPI]: Status: Passed
[15:33:12] [RadarAPI]: Opening Board Control Port()
[15:33:12] [RadarAPI]: Status: Passed
[15:33:13] [RadarAPI]: ar1.FullReset()
[15:33:13] [RadarAPI]: Status: Passed
[15:33:13] [RadarAPI]: Closing Board Control Port()
[15:33:13] [RadarAPI]: Status: Passed
[15:33:13] [RadarAPI]: Closing Gpio Control Port()
[15:33:13] [RadarAPI]: Status: Passed
[15:33:13] [RadarAPI]: ar1.SOPControl(2)
[15:33:13] [RadarAPI]: Status: Passed
[15:33:14] [RadarAPI]: ar1.Connect(7,921600,1000)
[15:33:17] [RadarAPI]: Warning: Connected with baudrate 115200
[15:33:18] [RadarAPI]: Warning: Disconnected existing BaudRate
[15:33:18] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[15:33:19] [RadarAPI]: ar1.Calling_IsConnected()
[15:33:21] [RadarAPI]: ar1.SelectChipVersion("IWR6843")
[15:33:21] [RadarAPI]: Status: Passed
[15:33:21] [RadarAPI]: ar1.frequencyBandSelection("60G")
[15:33:21] [RadarAPI]: ar1.SelectChipVersion("IWR6843")
[15:33:21] [RadarAPI]: Status: Passed
[15:33:21] Device Status : IWR6843/QM/SOP:2/ES:2
[15:33:21] [RadarAPI]: ar1.SaveSettings('C:\Users\Hao Nan\AppData\Roaming\RSTD\ar1gui.ini')
[15:33:23] [RadarAPI]: ar1.ReadRegister(0xffffe214, 0, 31)
[15:33:23] [RadarAPI]: ar1.ReadRegister(0xffffe210, 0, 31)
[15:33:23] [RadarAPI]: ar1.frequencyBandSelection("60G")
[15:33:24] [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31)
[15:33:24] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr68xx_radarss.bin")
[15:33:24] [RadarAPI]: Downloading BSS ROM RPRC Binary..
[15:33:31] [RadarAPI]: ar1.GetBSSFwVersion()
[15:33:31] [RadarAPI]: BSSFwVersion:(06.02.00.06 (22/08/19))
[15:33:31] BSS FW Download Success
[15:33:31] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr68xx_masterss.bin")
[15:33:31] [RadarAPI]: Downloading MSS RPRC Binary..
[15:33:34] [RadarAPI]: ar1.GetMSSFwVersion()
[15:33:34] [RadarAPI]: MSSFwVersion:(02.00.00.03 (27/08/19))
[15:33:34] MSS FW Download Success
[15:33:38] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[15:33:38] Status: Failed, Error Type: RESP TIMEOUT
[15:33:43] MSS Power Up async event was not received!

 

I read the comments from this thread (http://e2e.ti.com/support/sensors/f/1023/t/770709?DCA1000EVM-problem-encountered-when-using-with-mmWave-Studio-2-0-0-2-and-IWR6843ISK-MMWAVEICBOOST-combo) to make sure I had the correct HW configuration. 

Any clue on this or is there anything I should change?

Thanks!