This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA900: PGA900

Part Number: PGA900

Dear sr


if I supply  the PGA900 with 3.3V what will be the consumption of this component?

Can be my mistake but I did not find this information in datasheet of PGA900.

Regards

  • Hello,

    The power consumption depends on the operating mode and the voltage. The current consumption for different operating modes is shown in the datasheet. The normal operating current with no load on VBRG, no load on DAC, and an operating frequency of 1Mhz is 2.6mA (~8.5mW at 3.3V). Programming EEPROM, outputting through the DAC, increasing the M0 frequency, or supplying power to a bridge sensor will all increase the current consumption.

    Regards,