Other Parts Discussed in Thread: AWR1642, AWR1843
I need to run lab 10 in the automotive toolbox which named " lab0010_occupancy_vitalsigns_detection" on AWR1843 EVM. When I used the bin file of AWR1642 attached with the lab, it flashes and works but the results are not accurate due to the change in antennas and configurations between AWR1642 and AWR1843 EVMs. I checked another lab that contains MSS, DSS , and project specs for both EVMs and noticed the change between them and applied these changes in the lab. The build and the flashing had been done normally but I got an error "Start sensor error with -1".
I tried to run the lab in the debug to see what happens,I received the following errors (Error: MMWDemoDSS Unable to open the ADCBUF driver. Error : MMWDemoDSS Data Path init failed with Error [-1]).
Important note : When I also tried to rebuild this lab (without any modification in the files), I received the same errors. I don't know why the bin file of AWR1642 attached with the lab runs normally but the generated bin file after building does not work although the DSS and MSS projects are successfully built.
Thanks,
Abdelrahman