Other Parts Discussed in Thread: AWR1642BOOST,
Hi,
I have one AWR1642BOOST EVM (ES2.0) and one DCA1000 EVM. Earlier, I was using mmwave Studioe 02.00.00.02 and FPGA version was 2.7. I am using it on a Dell Laptop with windows 10 OS.
Then I installed latest mmwave Studio 02.01.00.00. I updated the FPGA binary as advised in section 9 of document DCA1000 EVM Data Capture Card (spruij4a.pdf). I followed all the steps as advised. The Lattice Diamond Standalone Programmer 3.10 64-bit Windows was used and in the end it showed successful operation.
Then I tried to use mmwave Studio 02.01.00.00. Where and when required, I allowed access through Windows Firewall. (I even attempted disabling Windows Firewall altogether).
I have set the IP address as advised in mmwave Studio User Guide. However, in "Sensor Config" tab, when i click "Setup DCA1000" button and then I click "Connect, Reset and Configure", then after that the output console of mmwave Studio shows error " Unable to read FPGA Version. [error -5] "
The "Output Log" is attached as text file to this message.
GM: Constructor GM: Wed Dec 18 17:17:09 2019 RSTD.Transmit("/Settings") [17:17:10] [17:17:10] ### Running Startup script: "C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Scripts\Startup.lua" ### [17:17:10] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1") [17:17:10] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss") [17:17:11] Scripter ignored: Attempt to UnBuild() again or before Build. [17:17:11] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll") [17:17:11] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE") [17:17:11] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE") [17:17:11] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE") [17:17:11] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE") [17:17:11] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE") [17:17:11] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\RunTime\\SAL.dll") [17:17:11] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "") [17:17:11] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE") [17:17:11] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1") [17:17:11] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE") [17:17:11] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE") [17:17:11] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false") [17:17:11] RSTD.Transmit("/") [17:17:11] RSTD.SaveSettings(): Settings saved to "C:\Users\Admin\AppData\Roaming\RSTD\config.xml" [17:17:11] RSTD.Build() [17:17:11] RSTD.SaveSettings(): Settings saved to "C:\Users\Admin\AppData\Roaming\RSTD\config.xml" [17:17:11] RSTD.Transmit("/") [17:17:11] RSTD.AL_Build() [17:17:11] RSTD.AL_LoadXml() [17:17:11] RSTD.Transmit("/") [17:17:11] RSTD.AL_Init() [17:17:11] RSTD.Clients_Build() [17:17:11] GM: Init [17:17:11] GM: Loaded 'C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Clients\\LabClient.dll' [17:17:11] GM: 1 Guest (s) init [17:17:11] GM: 1 Module(s) init [17:17:11] GM: 2 Tab (s) init [17:17:11] RSTD.Client_LoadXml() [17:17:12] [RadarAPI]: ar1.selectRadarMode(0) [17:17:12] [RadarAPI]: Status: Passed [17:17:12] Matlab Runtime Engine is installed [17:17:12] [RadarAPI]: Starting Matlab Engine.. [17:17:42] [RadarAPI]: Matlab Engine Started! [17:17:45] [RadarAPI]: ar1.selectCascadeMode(0) [17:17:45] [RadarAPI]: Status: Passed [17:17:45] [RadarAPI]: ar1.LoadSettings('C:\Users\Admin\AppData\Roaming\RSTD\ar1gui.ini') [17:17:45] TESTING = false [17:17:45] RstdNet: Port 2777: Listening.. [17:17:45] [17:17:45] ***Script completed successfully.*** [17:18:12] [RadarAPI]: ar1.frequencyBandSelection("77G") [17:18:14] [RadarAPI]: ar1.SelectChipVersion("AR1642") [17:18:14] [RadarAPI]: Status: Passed [17:18:14] [RadarAPI]: ar1.deviceVariantSelection("XWR1642") [17:18:14] [RadarAPI]: Status: Passed [17:18:18] [RadarAPI]: Opening Gpio Control Port() [17:18:18] [RadarAPI]: Status: Passed [17:18:19] [RadarAPI]: Opening Board Control Port() [17:18:19] [RadarAPI]: Status: Passed [17:18:20] [RadarAPI]: ar1.FullReset() [17:18:20] [RadarAPI]: Status: Passed [17:18:20] [RadarAPI]: Closing Board Control Port() [17:18:20] [RadarAPI]: Status: Passed [17:18:20] [RadarAPI]: Closing Gpio Control Port() [17:18:20] [RadarAPI]: Status: Passed [17:18:20] [RadarAPI]: ar1.SOPControl(2) [17:18:20] [RadarAPI]: Status: Passed [17:18:26] [RadarAPI]: ar1.Connect(4,921600,1000) [17:18:29] [RadarAPI]: Warning: Connected with baudrate 115200 [17:18:30] [RadarAPI]: Warning: Disconnected existing BaudRate [17:18:30] [RadarAPI]: Warning: Trying to connect with baudrate 921600 [17:18:31] [RadarAPI]: ar1.Calling_IsConnected() [17:18:33] [RadarAPI]: ar1.SelectChipVersion("AR1642") [17:18:33] [RadarAPI]: Status: Passed [17:18:33] [RadarAPI]: ar1.SelectChipVersion("XWR1642") [17:18:33] [RadarAPI]: Status: Passed [17:18:33] Device Status : XWR1642/ASIL-B/SOP:2/ES:2 [17:18:33] [RadarAPI]: ar1.SaveSettings('C:\Users\Admin\AppData\Roaming\RSTD\ar1gui.ini') [17:18:48] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\radarss\\xwr16xx_radarss.bin") [17:18:48] [RadarAPI]: Downloading BSS Patch RPRC Binary.. [17:18:50] [RadarAPI]: ar1.GetBSSFwVersion() [17:18:50] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17)) [17:18:51] [RadarAPI]: ar1.GetBSSPatchFwVersion() [17:18:51] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19)) [17:18:54] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\masterss\\xwr16xx_masterss.bin") [17:18:54] [RadarAPI]: Downloading MSS RPRC Binary.. [17:18:56] [RadarAPI]: ar1.GetMSSFwVersion() [17:18:56] [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19)) [17:18:59] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0) [17:18:59] [RadarAPI]: Status: Passed [17:19:00] MSS power up done async event received! [17:19:04] [RadarAPI]: ar1.SelectChipVersion("AR1642") [17:19:04] [RadarAPI]: Status: Passed [17:19:04] [RadarAPI]: ar1.SelectChipVersion("XWR1642") [17:19:04] [RadarAPI]: Status: Passed [17:19:04] Device Status : XWR1642/ASIL-B/SOP:2/ES:2 [17:19:04] [RadarAPI]: ar1.RfEnable() [17:19:04] [RadarAPI]: Status: Passed [17:19:04] BSS power up done async event received! [17:19:04] [RadarAPI]: ar1.GetMSSFwVersion() [17:19:04] [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19)) [17:19:05] [RadarAPI]: ar1.GetBSSFwVersion() [17:19:05] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17)) [17:19:05] [RadarAPI]: ar1.GetBSSPatchFwVersion() [17:19:05] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19)) [17:19:18] [RadarAPI]: ar1.ChanNAdcConfig(1, 0, 0, 1, 0, 0, 0, 2, 2, 0) [17:19:18] [RadarAPI]: Status: Passed [17:19:23] [RadarAPI]: ar1.LPModConfig(0, 0) [17:19:23] [RadarAPI]: Status: Failed, Error Type: REGULAR ADC MODE NOT SUPPORTED IN 5 MHz PART VARIANT DEVICE [17:19:32] [RadarAPI]: ar1.RfInit() [17:19:32] [RadarAPI]: Status: Passed [17:19:32] RF Init async event received! [17:19:32] [RadarAPI]: Time stamp, Temperture: 28060,40; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 0, 0; RxIQMM Status, Update: 1, 1; [17:19:43] [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0) [17:19:43] [RadarAPI]: Status: Passed [17:19:44] [RadarAPI]: ar1.LvdsClkConfig(1, 1) [17:19:44] [RadarAPI]: Status: Passed [17:19:49] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0) [17:19:50] [RadarAPI]: Status: Passed [17:20:04] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30) [17:20:04] [RadarAPI]: Status: Passed [17:20:10] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0) [17:20:10] [RadarAPI]: Status: Passed [17:20:12] Test Source Already Disabled...!!! [17:20:12] [RadarAPI]: ar1.DisableTestSource(0) [17:20:12] [RadarAPI]: Status: Passed [17:20:12] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1) [17:20:12] [RadarAPI]: Status: Passed [17:20:17] [RadarAPI]: ar1.GetCaptureCardDllVersion() [17:20:17] [RadarAPI]: Sending dll_version command to DCA1000 [17:20:17] [RadarAPI]: [17:20:17] DLL Version : 1.0 [17:20:17] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000") [17:20:17] [RadarAPI]: Status: Passed [17:20:23] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098) [17:20:23] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30) [17:20:23] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25) [17:20:23] [RadarAPI]: Sending fpga command to DCA1000 [17:20:34] [RadarAPI]: [17:20:34] FPGA Configuration : [17:20:34] Timeout Error! System disconnected [17:20:34] [RadarAPI]: Sending record command to DCA1000 [17:20:44] [RadarAPI]: [17:20:44] Configure Record : [17:20:44] Timeout Error! System disconnected [17:20:44] [RadarAPI]: ar1.GetCaptureCardFPGAVersion() [17:20:44] [RadarAPI]: Sending fpga_version command to DCA1000 [17:20:54] [RadarAPI]: [17:20:54] [17:20:54] Unable to read FPGA Version. [error -5] [17:20:54] [17:22:05] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098) [17:22:05] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30) [17:22:05] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25) [17:22:05] [RadarAPI]: Sending fpga command to DCA1000 [17:22:16] [RadarAPI]: [17:22:16] FPGA Configuration : [17:22:16] Timeout Error! System disconnected [17:22:16] [RadarAPI]: Sending record command to DCA1000 [17:22:26] [RadarAPI]: [17:22:26] Configure Record : [17:22:26] Timeout Error! System disconnected [17:22:26] [RadarAPI]: ar1.GetCaptureCardFPGAVersion() [17:22:26] [RadarAPI]: Sending fpga_version command to DCA1000 [17:22:36] [RadarAPI]: [17:22:36] [17:22:36] Unable to read FPGA Version. [error -5] [17:22:36] [17:26:52] RSTD.ShowLogFile()
Can you please guide what is the problem and how can I solve it to use AWR1642BOOST + DCA1000 EVM with mmwave Studio 02.01.00.00 and FPGA version 2.8 ?
As a further step to re-check, I re-installed FPGA version 2.7 using the same steps and it worked fine with mmwave Studio 02.00.00.02. I then again attempted to use FPGA version 2.8 with mmwave Studio 02.01.00.00, but again had same failure.
Thanks in advance for your help.